3/5/2020 9:47 AM | |
Joined: 9/30/2016 Last visit: 6/12/2024 Posts: 913 Rating:
|
Please also see the attached screenshots. I need to program and install 2 KTP700 Basic panels showing an number in percent (Akkumulator Position). I have the screens available in another panel but these panels have additional displays which are not needed in the 2 new ones. So - what is the meaning of Number respectively Screen number)? How do I move the 2 "Akkumulator Position" pics to position 1 and 2 (also Button 1 and 2)? How do I put the correct text on the buttons? Could I just delete the "Alarm", Dancer" and "Samkoring" pics if I don't need them? AttachmentKF16 Akkum.zip (38 Downloads) |
Follow us on