5/29/2018 2:10 PM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating: (6) |
I have a project with some small modifications - in one "normal" FC block and on safety FC block. When I download the modifications (the safety clock is downloaded with the safety editor) and try to run the machine I have lost the profibus communication to one of the 4 drives. And I have neither made any HW modifications, compiled the HW configuration or DL'ed the HW configuration. When I download the "old" version of the two blocks the machine is working again with communition to all 4 drives. What can be the cause of the fault and how do I troubleshoot to find it - and how do I correct it? AttachmentProfibus Error.zip (52 Downloads) |
Follow us on