5/1/2024 7:51 AM | |
Joined: 10/30/2022 Last visit: 10/26/2024 Posts: 1 Rating: (0) |
Hi, Is it also possible to establish a connection to instance of PLC sim with an S7-300? I Currently have a Wincc Unified project in TIA V19 with an MTP1500 and a proxy PLC which represents an existing 319 F-3 programmed in Simatic manger. I would like to run PLCsim from Simatic manager and let this communicate with the MTP1500 simulation. I already played around with NetToPLCSim but i was unable to make it work. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2024 09:06:09New subject after splitting |
|
Follow us on