5/28/2009 7:55 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating: (94) |
Hi samkcr, The question is very generic. There is lot of information on time synchronization available on this site. To help you on this the following information will be helpful
Have a look at this manual for PCS7 ontime synchronization. Even though you are using PLC-WinCC, the fundamentals remain same and you can use this to "plan" and get started. Hope it helps.
|
6/2/2009 7:24 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, Perhaps following FAQ will be useful - How can you set the time of an S7 controller from WinCC? There you'll find tricks for time-of-day synchronization via Industrial Ethernet. Hope this will helps. Best regards Hristo Mihalev |
6/2/2009 3:39 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi that FAQ is not a syncronisation, it is a time set.The times in PC and S7 can have differnces up to 500ms. The two linked FAQsare real time syncronisations. regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
6/2/2009 9:58 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating: (94) |
I will suggest that you keep your OS server as Time master. It is standard recommendation as well. I believe there is at least one confusing blunder in the above mentioned manual which complicates things.HenceI have extracted and attached the relevant pages from the original manual. (Ignore the page numbers at bottom)
Certain alarm messages may not be available in your case as you are doing a wincc-step 7 configuration and not PCS7. Point to remember:
Hope it helps...
AttachmentTime.zip (1004 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on