11/4/2014 8:42 AM | |
Joined: 4/24/2006 Last visit: 5/6/2024 Posts: 8634 Rating: (1149) |
Hello Daniel Carreira, The license should be on the panel. Please have a look at the following links: how can you transfer licenses to an operator device with the ALM withour WinCC flexible being installed? What should you watch out with regard ro licenses for WinCC flexible and panels? Best regards, Wizard |
11/4/2014 12:57 PM | |
Posts: 13 Rating: (0) |
Thanks for your help! |
This contribution was helpful to1 thankful Users |
6/11/2018 9:05 PM | |
Joined: 5/6/2010 Last visit: 5/5/2024 Posts: 1965 Rating: (272) |
Hello Pav1, if you have a new one TP1200 Generation 2 then you don't need the extra license at the panel, this license is included. At a "older" TP1200 you can transfer the license with the ALM. Hope this is helpful regards |
Last edited by: Jen_Moderator at: 6/21/2018 1:32:00 PMOptimized link. |
|
9/25/2018 11:30 AM | |
Posts: 3 Rating: (0) |
Hi, I do have problems with transferring Smart@server license to TP1200 Comfort panel (6AV2 124-0MC01-0AX0). I tried to use procedure described in the post: (https://support.industry.siemens.com/cs/document/74796111/what-information-is-available-about-licenses-for-wincc-(tia-portal)-?dti=0&lc=en-WW) but it didn't help :( I do literally miss both options "view->administration" and "Connect Target System". Please see attached screenshots for details. I do use Ethernet interface for connection and I do manage to ping panel from PC and viceversa (ping PC from panel when TP1200 in transfer mode). I tried both version of ALM, 5.3 and 6.0. Both have missing option. I do not have an Engineering station so I do not have any other Siemens software except of ALM on PC which I am using. What to do to install that license? Do I need to install something more in addition to ALM? Thanks in advance :) Regards, Daniel AttachmentScreenshots from ALM.pdf (520 Downloads) |
9/25/2018 12:04 PM | |
Posts: 3 Rating: (0) |
Hi, I tried to find this option many times :) Problem is that I do not have that option (please see attached screenshots). I made a query at forum as I don't know what I need to do to have that option available in ALM. Regards, Daniel AttachmentScreenshots from ALM.pdf (429 Downloads) |
9/25/2018 12:24 PM | |
Joined: 4/24/2006 Last visit: 5/6/2024 Posts: 8634 Rating: (1149) |
Hello, Have you installed the software 'Prosave'? Best regards, Wizard |
9/25/2018 12:29 PM | |
Posts: 3 Rating: (0) |
Hi, No. I do have only ALM. Nothing else. Do I need Prosave? Is there any particulary vesrion or any is good? Regards, Daniel |
Follow us on