7/5/2011 12:53 PM | |
Posts: 7 Rating:
|
Hi Expert/all I have some technical doubts reg FM354 pls clarify... (1) How many FM354 can be used in one S7300 rack ? other questions are splitted to suppose we use 5 FM354 in one rack...is it possible to run each axis at different feed rates in linear interpolation at the same time. is it possible to write into R-parameters of individual FM354 using PLC program and from DB?. is it possible to use bigger OPs like MP277 10" as graphical interface between user and FM354. pls calrify at the earliest. regards, jeetu |
Last edited by: O_Moderator at: 7/6/2011 2:46 PMsubject edited |
|
7/14/2011 10:02 AM | |
Joined: 4/24/2008 Last visit: 1/15/2025 Posts: 213 Rating:
|
Amaximum number is not known to me, but it is possible to use 5 FMs in one rack. |
|
|
7/14/2011 10:06 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hello, According to the type of CPU, take a look at its Technical Data. (example CPU317-2PN/DP max. FM modules are 8). I think this is implemented also in hardware confuguration in Step7. Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 7/14/2011 10:07 AM |
|
7/18/2011 11:38 AM | |
Posts: 7 Rating:
|
I tried it with H/W configurator....... I kept a CPU 315-2DP and installed 6, FM354s in slots 4 to 9...and when i compiled no errors reported...... |
Follow us on