12/8/2014 1:14 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello SIS AN, Hardnet-Adapters are called so, because additional hardware is used. CP1613 A2, CP1623 and CP1628 have a small computer on its board. see: http://support.automation.siemens.com/WW/view/en/62607733 Softnet-Adapter are "common" Network-Adapters, they do not have an additional computer on board, they are controled by the CPU of the PC. With Softnet you can have up to 64 connections. You can use a lean-license, if you have not more then 8 connections, otherwise you need a full softnet-license. With Hardnet you can have up to 60 connections. You need a hardnet-license. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to
2 thankful Users |
12/11/2014 8:26 AM | |
Posts: 49 Rating:
|
dearbg2492, Summary, with IE card( ethernet onboard), How many connections this card do? Any licence for this case? Thks alot.
|
12/11/2014 8:45 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello SIS AN, hier the link to the Delivery Release for SIMATIC WinCC V7.3 and SIMATIC WinCC V7.3 ASIA http://support.automation.siemens.com/WW/view/en/97493192 In point 5.Ordering data you can find Excel-lists with available licences. If you do not know, which licences, you would need for your configuration, you should ask you local Siemens-Sales-Person. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
12/11/2014 9:58 AM | |
Posts: 49 Rating:
|
dearbg2492, I amembarrassed. In short, to me: 1. Softnet lean or sofnet full is for CP 1612 or ethernet card(onboard). 2. In the case, you use Ethernet card(onboard).IF you useWorkstation-OS like Windows 7, the max connection is 8, although you can Softnet full. IF you useServer-OS, the max connections is 60, although you useSoftnet full( 64 connections). In short, you use Ethernet card(onboard), it depends on both Which OS and Which Licence softnet. 3. IF you use CP card such as CP1612,CP1613, it only depends on which softnet or hardnet licence you use? 4. What's the different between Ethernet Card(onboard) and CP1612 card? Onboard depends on which OS(operation system), and CP1612 NOT. Thanks alot.
|
Last edited by: SIS AN at: 12/11/2014 10:00 AMLast edited by: SIS AN at: 12/11/2014 9:59 AM |
|
12/12/2014 4:45 AM | |
Posts: 49 Rating:
|
Dearbg2492, I read the manual, i see that hardnet licence supports to 120 connections. Hardnet support two protocols. So, i use 60 TCP/IP connections and 60 other connection for the same card CP.Is it rights? How many CP ethernet card in your computer? IF there are two cards, i can extend to 240 connections and i must buy two harnet licence. IS it ok? Thks
AttachmentWinCC Communication Manual P.58.pdf (214 Downloads) |
Follow us on