6/24/2021 6:48 PM | |
Joined: 10/26/2017 Last visit: 5/25/2023 Posts: 77 Rating:
|
how many watt resistor we need to connect ?if 4 to20ma to 0 to 10 v we need to use 500ohms resistor.. what abot watt of the resistor? .2watt resistor enough ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/25/2021 08:22:41New subject after splitting |
|
6/25/2021 4:20 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating:
|
Hello, I can recommend to be in problematic here (external site): allaboutcircuits DC problematic Improve your knowledge there, it will be big benefit for you. |
With best regards... |
|
6/25/2021 5:18 PM | |
Joined: 10/26/2017 Last visit: 5/25/2023 Posts: 77 Rating:
|
Thank You very much Duris..
|
6/28/2021 9:44 AM | |
Joined: 10/7/2005 Last visit: 7/25/2024 Posts: 3011 Rating:
|
Be mindful too that 4-20mA over a 500 Ohms resistor will give you 2-10V (NOT 0-10V) so you'll need to consider this in your AI scaling. Resistor tolerance (which can be up to 20% for cheap ones) will also affect your result. All up, I would recommend to add a 4-20mA AI card to the S7 and do it "properly" |
Cheers |
|
This contribution was helpful to
2 thankful Users |
Follow us on