12/7/2023 2:28 PM | |
Joined: 10/11/2006 Last visit: 5/22/2024 Posts: 5849 Rating: (793)
|
Hello, here is an example for cyclic SINAMICS S120 with a SIMATIC S7-1500https://support.industry.siemens.com/cs/ww/en/view/109749224 and acyclic communication Acyclic Data Exchangehttps://support.industry.siemens.com/cs/ww/en/view/109479553 |
With best regards, |
|
12/11/2023 11:03 AM | |
Joined: 10/11/2006 Last visit: 5/22/2024 Posts: 5849 Rating: (793)
|
Hello, when it is enough to read 89 (voltage) in a cycle of 500 or 1000 ms, I would choose Acyclic Data Exchange2.2.3 FB LAcycCom_ReadDriveParams (FB 30512) Using the function block LAcycCom_ReadDriveParams a parameter dataset with several parameters can be read from a SINAMICS drive object or a PROFIdrive profile compliant drive. https://support.industry.siemens.com/cs/ww/en/view/109479553 |
With best regards, |
|
Follow us on