4/14/2023 9:53 AM | |
Joined: 1/1/2023 Last visit: 4/14/2023 Posts: 3 Rating: (0) |
Greetings, I am new to Siemens Logo PLCs and I need your assistance. I have a project file that I want to upload to my Logo PLC (0BA5), but it says it is incompatible because it was created with the default settings in Hardware type (LOGO! 8.3). How can I change the hardware type so that I can upload the program to my PLC without redoing the whole project? I have attached the program and the hardware type options for your reference. Appreciate your help AttachmentLOGOBooster_v2_2_10.zip (300 Downloads) |
4/14/2023 10:17 AM | |
Joined: 12/18/2014 Last visit: 10/19/2024 Posts: 33999 Rating: (4228)
|
I don't know why you make a again a topic for the same problem. You ask the same for your problem in this topic: How to change hardware type from LOGO! 8.3 to Logo 0BA5In your first topic have you became all answers. And for the future: Don't post twice for the same topic. |
4/14/2023 10:27 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject How to change hardware type from LOGO! 8.3 to Logo 0BA5 is published within the conference LOGO! - Software. Jen_Moderator |
This contribution was helpful to1 thankful Users |
Follow us on