8/18/2015 2:47 PM | |
Posts: 457 Rating: (46) |
Hello, Here you will find a youtube video regarding S7-1200 and HMIs: https://www.youtube.com/watch?v=-Au6m45GIvA
Best regards Georg |
8/18/2015 3:45 PM | |
Posts: 15 Rating: (0) |
the HMI does already exist the PLC (1214C V 3.0) exists as well but i can't run simulation because i use TIA portal V13 and this version of 1214C is not working under TIA V13 So i added a new PLC (1214C V 4.1) that is working fine under tia v13 My problem is: When i connect my HMI (simulated one) to this 1214C V 4.1 and then i compile, it gives me errors and says that the HMI and the CPU are not connected to same subnet but in fact they are So how can i connect this new PLC to this HMI that does already exists ?? please check out the attachments Thank you all AttachmentHMI and PLC connection.pdf (1022 Downloads) |
9/9/2015 10:33 AM | |
Joined: 5/12/2006 Last visit: 10/15/2024 Posts: 22413 Rating: (3017) |
in the properties if the HMI Connection. |
Follow us on