1/31/2021 6:56 PM | |
Posts: 1 Rating: (0) |
Hi, i want to ask if it is possible to change screen in HMI using timers. This is my first time doing it so i don't really know if this is the correct way of doing . My plan is to change screen once the TON reaches for example 2 second and then the HMI screen will change to another screen. Any kind souls can help me out? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/01/2021 05:52:04New subject after splitting |
|
9/9/2021 1:47 AM | |
Joined: 7/29/2021 Last visit: 5/24/2024 Posts: 1 Rating: (0) |
I have the same question |
9/9/2021 8:16 AM | |
Joined: 4/24/2006 Last visit: 8/7/2024 Posts: 8711 Rating: (1166) |
Hello, In addition to the answer of Mr.V. Have a look at the following link: How do you configure a screen change via the controller in WinCC (TIA Portal)? Best regards, Wizard |
Follow us on