10/11/2023 11:17 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (821)
|
Hello, don't have still experience with DALI but for what reason is there that short address parameter? Your TIA version? Can you be kind post screenshots of other parameters from doc? ZIP more screenshots in case. I can recommend this Example: Commissioning of ET200SP with DALI CM |
Last edited by: Duris_I at: 10/11/2023 11:30:00With best regards... |
|
10/11/2023 11:23 PM | |
Joined: 9/14/2023 Last visit: 11/1/2023 Posts: 6 Rating: (0) |
Hi, yeah I'm not very proficient with DALI either. I'm using TIA 18.1. As far as my understanding goes short address is 0,1,2...63. It's an individual address of the devices connected to the card. ET 200SP Communication module CM 1xDALI (6ES7137-6CA00-0BU0) (siemens.com) I'm looking through the commissioning example, a bit confusing for now. AttachmentET_200_SP_CM_1xDALI_en-US_en-US.pdf (400 Downloads) |
Last edited by: Jen_Moderator at: 10/12/2023 05:34:15PDF attached from link. |
|
10/12/2023 5:20 AM | |
Joined: 9/14/2023 Last visit: 11/1/2023 Posts: 6 Rating: (0) |
I think I'll just go with a FOR DO loop, not sure if I should use LAD for this or SCL |
Follow us on