1/4/2013 1:57 PM | |
Posts: 31 Rating:
|
Dear sir, please find here with attachment of source code. Warm Regards, Srinath AttachmentMODBUS_SEND_RCV.zip (702 Downloads) |
1/4/2013 7:44 PM | |
Posts: 3093 Rating:
|
Hello Srinath, Break on the receiving line is reported in the first cycle when calling P_SND_RK. So you won't get a positive edge to continue. I'd prefer a solution which has not got that amount of Start and Send bits. I copied thebitsof DB40 from the standard Modbus sample. Of course you can use flags instead. The suggestion is no complete program. It is just an idea how you could realise it. Some things are only comments, no code. Regards, Kaulquappe AttachmentD:\temp\suggestion.pdf (682 Downloads) |
Last edited by: Kaulquappe at: 1/4/2013 7:49 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on