2/12/2011 12:05 PM | |
Joined: 6/27/2008 Last visit: 7/6/2021 Posts: 43 Rating: (4) |
Are you using chronological messaging (ALARM_8, etc. ) or bit alarm procedure or the analog alarms ? In case ofchronological messaging you have to put a group display in each picture level. For example you have area button AREA1 and in that area top level picture PIC1 and lower level pictures PIC1_A, PIC1_B. If you want messages to be transfered from PIC1_A and PIC1_B to AREA1 button, you have to put a two group displays in PIC1 and connect one to PIC1_A and other to PIC1_B (using dynamic wizard connect group display to the picture). And of course you have to have objects (like faceplates) with group displays in PIC1_A and PIC1_B. http://support.automation.siemens.com/WW/view/en/674987 If you are using bit alarm procedure read |
Last edited by: Gedas at: 2/12/2011 12:21 PM |
|
This contribution was helpful to2 thankful Users |