9/9/2009 1:00 PM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User banoe81 wrote: Dear All,so have you ever get data from sentron pac 3200 directly through from WInCC v7.0? if any one have sucessfully trying win CC v 7.0 modbus tcp with sentron pac 3200 .please give me solution....i already make chanel modbus TCP/IP # 1,cpu type Premium,Micro,server = ip addres sentron pac 3200 (192.168.100.45) port 502,addres remote slave 1.....after that i make tag using name freq_1 using floating number 32-bit iee 754 adress= 55 (index freq for modbus at pac 3200 is 55) adapt format =float to float...are my setting already complete?please give me advise...thanks . |
Last edited by: CS Moderator at: 9/15/2009 11:54 AM |
|
9/9/2009 3:27 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating:
|
Hello, Look at Displaying values of the SENTRON PAC3200 / PAC4200 in WinCC 7.0 SP1 via Ethernet Hope this will helps. Best regards, Hristo Mihalev |
Last edited by: O_Moderator at: 6/28/2010 7:29 AMlink edited |
|
9/12/2009 3:57 AM | |
Joined: 9/2/2009 Last visit: 4/2/2024 Posts: 11 Rating:
|
Thanks alot UMENCHO i'll try it |
9/14/2009 1:13 PM | |
Joined: 9/2/2009 Last visit: 4/2/2024 Posts: 11 Rating:
|
hai , i have try,but still not worked this is the file that i have already try. AttachmentPAC3200 setting.pdf (1529 Downloads) |
6/27/2010 4:38 PM | |
Joined: 4/2/2008 Last visit: 10/4/2023 Posts: 4 Rating:
|
is this problem with wincc 7.0 modbus problem resolved or not? |
6/28/2010 6:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hi UMENCHO, When I click on above link following message is displayed, "you are not authorised to open this link." Why is it so?Is it protected one. Can you help? DEEP. |
Last edited by: O_Moderator at: 6/28/2010 7:29 AMlink edited |
|
9/6/2010 9:17 PM | |
Joined: 2/18/2010 Last visit: 8/2/2024 Posts: 3 Rating:
|
Hi , I tried the solution with wincc v7.0 sp1 for read some values and no problem. ButI can't write register. I found someone who as the same probleme at this link : https://www.automation.siemens.com/GB/tf/WW/en/Posts/43854 Thanks Best regards |
Follow us on