6/3/2011 8:21 AM | |
Joined: 5/28/2009 Last visit: 8/2/2024 Posts: 127 Rating:
|
Hi....Queries See the attachment..... AttachmentOPC_WinCC.zip (730 Downloads) |
Regards, |
|
This contribution was helpful to
1 thankful Users |
6/6/2011 7:16 AM | |
Posts: 7 Rating:
|
Dear All: That what I got ! (No tags is OPC Scout V10? Although I have made my tags in WinCC V7.0 SP1 and WinCC is in run state...) Please see the attachment.... Regards AttachmentSnapshots.zip (419 Downloads) |
6/6/2011 9:05 AM | |
Posts: 291 Rating:
|
Hello Queries, Please find the attachment!! (I do think that you need to do the related configuration if you're using "V6.x". BTW ~ While installing WinCC V7.x, it will modify all the related settings for us. We just need to press an "Apply" button popped up.)
Well ~ you may refere to: http://www.opcfoundation.org/ for more information. B.R., Komi AttachmentOPC_via_DCOM_e.pdf (583 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on