6/2/2023 4:48 AM | |
Joined: 5/15/2023 Last visit: 12/26/2023 Posts: 19 Rating:
|
Hello! It was possible to configure the Wago equipment (modules). At the moment, I have an error only in the case of connecting a load cell via CAN. In the documentation for the CAN module (wago 750-658), the error description is as follows: "The internal counter (receive direction) is greater than 127. The I/O module is initialized again."What causes this error? What needs to be done to solve the problem? Screenshots of errors in the TIA Portal attached.
AttachmentError.zip (339 Downloads) |
12/5/2023 2:25 PM | |
Joined: 5/15/2023 Last visit: 12/26/2023 Posts: 19 Rating:
|
Hello, dear. You were right from the very beginning, module 658 is not suitable for working in Tia portal, there is no support. That was the problem that I can't get the data, When working with the 658 module, there is no way to upload weight cell files to the Tia portal eds files. Here is a good example of how it should be SIMATIC PN/CAN LINK - CAN/ CANopen Commissioning - YouTubeIn the attachment in the picture you will see what I see |
Last edited by: The Helping Hand at: 12/06/2023 10:17:06Video embedded from link. |
|
This contribution was helpful to
1 thankful Users |
Follow us on