10/8/2008 4:29 PM | ||||
Joined: 4/24/2006 Last visit: 5/21/2024 Posts: 8650 Rating: (1151) |
Dear y.c. Do you mean S5-150U or S5-115U? I guess you have cable 6ES5 734-1BD20. Then you must have an adapter (9-pin female and 25-pin male)
Best regards, Wizard |
|||
10/9/2008 8:50 AM | |
Joined: 4/24/2006 Last visit: 5/21/2024 Posts: 8650 Rating: (1151) |
Dear y.c. Because you talk about S5-150U: Please have a look at this thread: /tf/WW/en/Posts/1158 And perhaps this is useful: http://support.automation.siemens.com/WW/view/en/217845 Best regards, Wizard |
10/14/2008 3:52 PM | |
Joined: 4/24/2006 Last visit: 5/21/2024 Posts: 8650 Rating: (1151) |
Hi y.c Perhaps the following link might help: http://support.automation.siemens.com/WW/view/en/13063839 Best regards, Wizard |
10/15/2008 10:42 PM | |
Posts: 487 Rating: (44) |
See the post by import-user-2 at /tf/WW/en/Posts/1158
This can be used as an adaptor on top of normal RS232-TTY converter. |
7/8/2015 1:28 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
Follow us on