Industry Online Support
Technical Forum
6/10/2010 7:44 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, Look at 611U Toolbox Included is a sample project that will allow you to operate the 611U positioning control unit as a basic positioner utilizing the traversing blocks. The toolbox includes an explanation of the special function block FB83 for use with 611U drives. FB83 is include in Step7 simple project which you could find there. More info plus documentation for 611U is available at www.automation.siemens.com/doconweb Best regards, Hristo Mihalev |
6/13/2010 1:01 PM | |
Posts: 3 Rating:
|
thanks Hristo Mihalev. It is very helpful. But need help to identify the memory location of DB 71,72 for reading and writing data. |
6/13/2010 2:26 PM | |
Joined: 9/18/2006 Last visit: 5/3/2024 Posts: 589 Rating:
|
Hi. Probably it will help you. It is my example. Best regards. |
This contribution was helpful to
2 thankful Users |
Follow us on