9/2/2019 6:03 AM | |
Joined: 5/22/2018 Last visit: 4/2/2024 Posts: 13 Rating: (0) |
Hi huggy, As per the client requirement, I have to use the same SCL code in TIA portal 1500 series CPU. So, I have migrated the project from STEP7 V5.5 (CPU414-5H) to TIA Portal V13 - (CPU414-5H). And no errors were found. An Error was found during Project conversion from TIA Portal V13 -(CPU414-5H) to TIA Portal V13 -(CPU1515-2PN). Ex: #RANGE_HI := DWORD_TO_REAL(#RANGE_HI_DB.DD[#Index * 4 t+ #DB_Start_Addr]); // BAD (This format is NOT accept (EX: "DD")) Please find the attached file for your reference. How to clear this error? Thanks & Regards, M.Prakash AttachmentSCL_Error.pdf (165 Downloads) |
Follow us on