1/17/2022 1:01 AM | |
Joined: 9/9/2013 Last visit: 4/18/2024 Posts: 2 Rating: (0) |
I need the following solution. Even trying to use the S88. There is EMT in production interconnected with other EMT's. However, when I need to do CIP in the plant, there is another EMT working in the valve Flip Production CMTs. In short, I need to use shared, and used other systems. Now with PCS7 and technology blocks, what would be the best way? How to create a CMT block with ShrdResL? How would I be able to read the status of the CMT valve, and give the command to the CMT ShrdResL? Or is it ideal to use everything as Strategy Control and fully normalize my documentation? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/17/2022 12:36:21New subject after splitting. |
|