11/9/2021 2:23 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (173) |
Dear Community, during the last week of October we have introduced a new function for creating new topics. With this feature, the creation of topics will be easier for all users who are not familiar with the structure of the conferences. The feature is integrated e.g. on the page Conference overview via the known button "New topic". Clicking the button will lead you to the following overlay: Here, the topic creator can use a drop-down menu to select the target conference for the new question or leave the assignment to the moderator. These unassigned topics are visible for the topic creator, experts and moderators. So, if you are not sure where to publish your next question feel free to use this new functionality. Best regards, |
This contribution was helpful to4 thankful Users |
Follow us on