3/20/2017 1:26 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, The bad news is that the error is not related to SFC only. Check the following link and see my last post of that topic. Maybe it helps you. I solved my error with the solution. |
Last edited by: Oreca at: 3/20/2017 1:27:56 PMIf I could help you, you can use the RATE button. Thank you. |
|
3/22/2017 9:46 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, It should be no problem if you try to delete the type when you have instances of it in your program, it just gives you an error message, so I think you already had a problem with the program. |
If I could help you, you can use the RATE button. Thank you. |
|
3/28/2017 4:25 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
The error code that shown in the topic seem related to my problem. After that, i tried to delete and recreate another s7 program as per recommendation. I found there are another problem arise during copying of chart to the new s7 program folder, which is insert (1739:20) Step does not exist (any longer). It happened to all my sfc type block. Seem that solution is not work for me too. Anyway, my ultimate solution solved my problem. I retrieved back my back up archive one days before and redo back all my modifications. Now i will check my step one by one to see which is the crucial step that cause the problem. And later, prevent the issue from happened again. Thanks. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/29/2017 8:24 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
I solved my issue, Note 1739:20. with PCS 7 V8.2 CFC Update 3. Reference thread PCS 7 V8.2. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on