4/11/2012 11:49 PM | |
Posts: 108 Rating:
|
Hi, I am currently working on a project that is using two PCs running WinCC V11 to provide the graphical interface to an alarms and monitoring system. Each PC will be displaying information across four monitors, in order to provide the same graphical interface to a total of eight locations. The same base screen in WinCC is placed on each of the four monitors using four independent screen windows. Pressing buttons down the left-hand side of the base screen changes the screen shown in a screen window that occupies the rest of the space on this screen. A diagram showing the layout of the base screen is attached. It is therefore possible, using a multiple-monitor configuration, to replicate the graphical interface on four monitors using only a single PC. However, the problem I have is that it should only be possible to acknowledge alarms from one of these eight monitors. This means that alarms should only be acnkowledgeable from one of the four monitors attached to one of the PCs. As far as I can tell though, there is no way of determining which monitor in a multiple-monitor system is being used. Is there a way to do this? Thanks for your help Jason AttachmentBaseScreen.pdf (608 Downloads) |
Follow us on