5/29/2011 7:28 AM | |
Posts: 691 Rating: (36) |
Dear SonNH There won't be a problem You ned to do engineering in Server PC then load it to Standby. And the Client will be accessing the server, So no need to do anything on the Client. In the field level, the PLC should be connected eith both the Servers. And client should access only servers. Have a look at the Pic Have a look at this also |
Last edited by: Shar at: 5/29/2011 7:32 AMLast edited by: Shar at: 5/29/2011 7:30 AM |
|
5/29/2011 9:23 AM | |
Posts: 50 Rating: (1) |
Thansk Shar. I know we only need to config OS Master server then load it to Standby server then OS Client access to server or standby server (if Master server down). So I want to display same graphic on both OS Master server, Standby server and Client. I don't need to do anything on the Client, are you sure? I need to create a graphic on Master server then load it to Standby server. How to load it to Client? |
5/29/2011 10:20 AM | |
Joined: 5/28/2009 Last visit: 5/5/2024 Posts: 127 Rating: (10) |
Hi....SonNH Any changes made in the engineering station and after then downloded to the servers will be reflacted in client. As because client gets pages from the servers. (Note: For first time you need to download in client. After this any changess you made on graphics in engineering station and downloded to the servers will automatically reflected in the client. You don't need to do any thing in the client. ) |
Regards, |
|
5/30/2011 8:55 AM | |
Joined: 10/3/2010 Last visit: 5/23/2024 Posts: 1552 Rating: (188) |
Or do you mean always having the same picture displayed on the client as on the server? |
B r g d s , |
|
5/30/2011 12:08 PM | |
Joined: 10/3/2010 Last visit: 5/23/2024 Posts: 1552 Rating: (188) |
off course I know that but the question is if SonNH wants his client to follow the displayed screen as actually shown on the server and if someone jumps to another picture on the server, that SonNH wants the client to make the same picture switch at the same time automatically. Don't think but just in case... |
B r g d s , |
|
Follow us on