7/6/2023 1:06 PM | |
Joined: 5/12/2022 Last visit: 7/2/2024 Posts: 4 Rating:
|
I am using TIA Openness to configure hardwares, I found an excellent example on Github but unfortunately it is not complete. I could generate devices and set IP addresses and also make connections under network view but under Topology view I could not make any connections since I haven't found the correct method for it. Does anyone know how to do port to port connections using TIA Openness API & Python? Has anyone succeeded it already? Please let me know. Here is the Code snippet I copied from Github:
------------------------------------------------------------------------------------------ |
Last edited by: mukara at: 07/06/2023 13:51:31Last edited by: mukara at: 07/06/2023 14:22:59Last edited by: mukara at: 07/06/2023 14:23:57Last edited by: Jen_Moderator at: 07/07/2023 09:04:35New subject after splitting |
|
7/10/2023 9:05 AM | |
Joined: 11/4/2011 Last visit: 7/4/2024 Posts: 226 Rating:
|
Hi there, I think this should be what you are looking for, connecting ports of devices: https://support.industry.siemens.com/cs/de/en/view/109815199/131679230603 Regards, |
6/29/2024 4:09 AM | |
Joined: 11/22/2017 Last visit: 7/3/2024 Posts: 3 Rating:
|
I have created project in TIA portal and added CPU, IM modules, Also Profinet IO system configured and IP address assigned I want to add I/O address to IO modules used in ET200SP, need support to identify the good syntax ? Here I have attached the codes for reference AttachmentPython_Tia Openness.txt (3 Downloads) |
Follow us on