6/17/2020 12:43 PM | |
Joined: 4/28/2015 Last visit: 3/14/2025 Posts: 398 Rating:
|
Hello, are you sure, that it is possible to use Yaskawa Sigma 3 drive with PTO...? What type of drive do you use? Do you use the right signal level? Maybe you need a option board (5V, 200kHz - 6ES7222-1AD30-0XB0) on S7-1200 to connect the drive... |
This contribution was helpful to
1 thankful Users |
Follow us on