4/10/2019 1:23 PM | |
Joined: 10/26/2017 Last visit: 5/25/2023 Posts: 77 Rating: (0) |
Hello, How to download project to runtime pc? how to create the pdata file ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/11/2019 10:46:52 AMNew subject after splitting |
|
4/11/2019 2:21 PM | |
Joined: 8/3/2009 Last visit: 4/30/2024 Posts: 12869 Rating: (1643)
|
Hello kmansal you are writing of a PDATA file so I suppose you have a WInCC Advanced Rutnime Project in TIA Portal. -> In this case you can do two way of loading: Online: -> if you are in the same network as the Runtime System then activate the Runtime loader on the RT PC and on the Engineering System use the Loading function Offline: https://support.industry.siemens.com/cs/de/en/view/109740696 there is also a small chapter to a PC Runtime Basically the fwx File (and the other pwx and so on ) are generated in the IM/HMI Folder in the TIA Portal Project if you compile your HMI Project. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
4/14/2019 2:46 PM | |
Joined: 10/26/2017 Last visit: 5/25/2023 Posts: 77 Rating: (0) |
I need to know the IP address for the SimaticPC (configured in TIA) and windows runtime PC need to be same ?? If we set different then how to download?
|
Follow us on