11/8/2010 12:19 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi SonNH, For your Configuration I suggest you the DP-DP Coupler, so in that it will work with all DP Master configuration. Have a look on the Manual, |
Ammy |
|
11/8/2010 1:53 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Yes, you can. My suggestion is: In the first (MPI) port to exchange data with one S7-300 (limited quantity of data). (MPI network http://support.automation.siemens.com/WW/view/en/747743). In othe other port (Profibus) to exchange data with S7-300 (like Profibus slave) or via DP/DP Coupler with S7-300 (like Profibus Master).(Profibus Network). Or in both ports to build Profibus network and to exchange data with slaves. (Profibus network). Of course you could have mix of both previous case if you add one interface card in 416-4 CPU. (MLFB 6ES7964-2AA04-0AB0INTERFACE MOD. DP-MASTER F. S7-400) BR, Hristo Mihalev |
Last edited by: UMENCHO at: 11/8/2010 1:56 PMLast edited by: UMENCHO at: 11/8/2010 1:54 PM |
|
11/9/2010 8:05 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello SonNH; I am afraid I do not exactly understand what you are trying to do here, but I will try to clear up a few issues. An I-slave is an "intelligent"Profibus-DP slave (based on an S7 CPU) that can exchange data with another I-slave, in a mechanism called "Direct data Exchange" (DDX), instead of having the DP master tranfer the data between the slaves. In the following FAQ, yuou will fing a great explanation of this DDX function, and a link to a sample project and a list of DDX-capable slaves. http://support.automation.siemens.com/WW/view/en/15196761 Now, if I have understood you well, you would like to have DDX between a slave CPU and ET 200M module. Based on the list of I-slaves mentionned eearlier, this is not possible. You could simply establish both the S7 CPu and the ET 200M as regular slaves to the Profibus master in your project. If I have not cleared up the issue, please come back with more detailed questions. Hope this helps, Daniel Chartier |
Follow us on