12/1/2023 12:02 AM | |
Posts: 1 Rating:
|
Hello everyone, I am trying to fill the space between two surfaces of a turbine blade, but I don't know which command to use. I imported a geometry made of several sections of the blade (in shape of an airfoil) connected to each other by two curves at leading and trailing edge. This is the 'external' surface. I created the internal surface with offset command and I need to fill the space in between these two surfaces in order to create the corrispondent solid afterwards. I don't think I can use 'BlueSurf', as the two surfaces aren't linked by any curves which I can select as 'Guide Curve'. I created the internal surfaces by offsetting the external surface of 50 mm towards the inner ; but I don't understand why near the trailing edge, the upper and lower part of the offset surface intercept to each other. Lastly, I wanted to ask how to join two lines in a single one. As you can see in the third photo, the trailing edge has been 'cutted' and so there is a small segment which doesn't allow the curve of that section to close completely. So I need to join these to lines. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/01/2023 06:25:01New subject after splitting |
|
12/1/2023 4:32 AM | |
Joined: 3/30/2020 Last visit: 4/3/2025 Posts: 5053 Rating:
|
Which product are you enquiring about? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
We are working on a new user interface with better overview and more relevance.
To explore the new Forum, you can follow the textbox in the right column, which will lead you to the corresponding page in the new Forum. Alternatively, you can start from the main page by following this link:
https://sieportal.siemens.com/en-ww/support/forum
In the coming days, we will update the configuration step by step, so that you are directed to the new Forum by default. The “classic Forum” will remain available for all known functionalities alongside the new one.
We are thrilled to finally share the future of our Forum with you. Thank you for your commitment!
Kind regards,
the Forum Support Team
Follow us on