6/28/2011 1:00 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Check the attachment for possible variable types which can be forces in S7300 and S7400.Please note, you can only modify a cell in a datablock,It is enough if it is not written from other part of program.To be sure,select the address,right click and select go to location. find more information in section 20.8 on forcing variables here; SIMATIC Programming with STEP 7 V5.5 Regards |
Last edited by: hdhosseini at: 6/28/2011 1:10 PM |
|
6/29/2011 7:02 AM | |
Joined: 6/28/2011 Last visit: 2/10/2024 Posts: 111 Rating: (0) |
My CPU is CPU 315-2DP. will it support the forcing of data block? |
6/29/2011 9:35 AM | |
Posts: 691 Rating: (36) |
You can modify the DB Values in any of the S7- CPU just like Memory Variables. |
6/29/2011 9:45 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Dear kuttysk If you are sure the DB114.DBX10.2 is only written from HMI, So you can set or reset it from HMI with user authentication procedure.I am afraid you can not force a cell in Data block! Regards |
Follow us on