7/24/2013 12:32 PM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello Shailesh The Command set posted by you already shows Delivery confirmation Msg received. This is how, I understand the Msg : ------------------------ AT+CSMP=49,167,0,0OK < Set Msg sending parameters> AT+CNMI=2,2,0,1,0 OK AT+CMGS="Mobile Number" > Message content (Ctrl+Z) < Send a Msg in Text Mode i.e. Send SMS > +CMGS: 72 OK < Successful Transmission> +CDS: 6,228,"Mobile Number",129,"08/10/22,10:08:35+32","09/10/22,10:08:38+32",0 < Messege was correctly delivered> +CMT: "Mobile Number",,"08/10/22,10:09:17+32" testing < New Msg Received> ----------------------- I would suggest that you download the AT command set manual of the Modem that you are using and check out the details of parious commands in the same. Here is a link of AT Command set Manual of Logicbus Modem that I had used for a similar application sometime back : http://www.logicbus.com.mx/pdf/31/Comandos_AT_generales.pdf Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
Follow us on