1/22/2008 7:15 AM | |
Posts: 11 Rating:
|
Hello, I have a server client configuration, 1 WinCC Server, 3 clients. WinCC V6.0 SP3 On my screens my client asks me if it's possible to enter start times for each day. The meaning is that my production line stops each day at a given hour and should automatically startup the next day. This means I have an array of TIME_OF_DAY values in my PLC. In the PLC, I can compare the startup time against the PLC system time and so, start up a furnace. My problem is now, How do I get these TIME_OF_DAY values from WinCC screen to the PLC ? Please advice, Regards, Tom |
1/22/2008 8:57 AM | |
Posts: 1776 Rating:
|
Hi, see the FAQ http://support.automation.siemens.com/WW/view/en/22531447 the FAQ is for datatyp Time. For the datatyp Time_of_day adapt the script. best regards |
Follow us on