10/26/2019 12:28 PM | |
Joined: 9/27/2006 Last visit: 5/21/2024 Posts: 12257 Rating: (2668)
|
Hello earthcitizen; Here is a Simatic Manager (Ste7 v5.x, for S7-300 and S7-400 PLCs) implantation of a numerical low-pass filter. It could be a basis for your own application: https://support.industry.siemens.com/cs/ww/en/view/6170416 Hope this helps, Daniel Chartier Edit: the following application note shows how to implement a Butterworth filter in s-domain in a PCS 7 environment. Even if the CFC code cannot be useful for your project, the accompanying document should prove interesting. https://support.industry.siemens.com/cs/ww/en/view/44908868 D.C. |
Last edited by: dchartier at: 10/26/2019 12:41:28Last edited by: dchartier at: 10/26/2019 14:14:12 |
|
This contribution was helpful to2 thankful Users |
10/26/2019 1:20 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359)
|
Hello,
Any S-Domain transfer functions can be implemented in PLCs,There is a topic as a solution in SCL: Numeric Methods to Solve ODEs(Ordinary Differential Equations )I hope it helps, hdhosseini |
This contribution was helpful to1 thankful Users |
10/29/2019 12:39 AM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (106) |
Butteworth filter, first order filter what's next? I will start with FIR filter and its application in my case. Few years ago I wanted to make measuring and generator protection device for small projects where customers didn't demand high quality generator protection devices as Siemens 7UM62 or ABB Reg615. I was looking for some product with capability of sampling voltage and current with at least 10kHz. Unfortunately Siemens still didn't release something like that, so I tried this : Beckoff EL3783 Terminal It is terminal for state monitoring of a 3-phase AC voltage system with sampling rate of 20kHz. The following properties are characteristic of the EL3783:
|
Last edited by: SOble at: 10/29/2019 00:41:05Last edited by: SOble at: 10/29/2019 00:42:59Last edited by: SOble at: 10/29/2019 00:45:24Last edited by: SOble at: 10/29/2019 00:47:25Last edited by: SOble at: 10/29/2019 00:51:52Last edited by: SOble at: 10/29/2019 09:11:25Last edited by: SOble at: 10/29/2019 09:16:42Mistake in sampling rates 100kHz to 10kHz and 200kHz to 20kHz Website: |
|