1/26/2024 2:15 PM | |
Joined: 9/14/2021 Last visit: 1/28/2024 Posts: 1 Rating: (0) |
Hello, I have same 2 proportional valve in our system. These valves work on IO link. I have separate distance sensor for feedback purpose of valve opening. I want to start these 2 valves at same flow rate (20% open spool), If one valve opening distance is higher than we need to increase the second valve flow rate to achieve the first valve distance. Please help us to what type of logic used for this. ------------------------------------------------------------------------------------------ |
Last edited by: A276 at: 01/26/2024 14:15:47Last edited by: Jen_Moderator at: 01/29/2024 09:28:16New subject after splitting |
|