6/16/2020 4:53 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, as an owner of the IOT2050 you might have recognized that there is no image pre-installed on the eMMC, as I promised here. The reason is that this Industrial OS version has a delay for release. So we decided to ship the hardware without. You will receive the SIMATIC Industrial OS as soon as it released. In the meantime you can use the Example Image and run it from a SD card or from the eMMc. Since the installation to the eMMc is not that easy I have created a document with a description. Best regards! AttachmentInstall_image_eMMc_V1.0.pdf (3412 Downloads) |
Last edited by: bergmanu at: 06/17/2020 13:21:21changed PDF - links can now be pressed Last edited by: bergmanu at: 06/17/2020 13:41:38added hint for not working link to example image Last edited by: bergmanu at: 06/24/2020 14:32:42Example is now online Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to3 thankful Users |
6/19/2020 5:09 PM | |
Joined: 8/20/2018 Last visit: 8/8/2024 Posts: 2 Rating: (0) |
How do I DM bergmanu for the new images? |
7/15/2020 4:08 AM | |
Joined: 4/28/2015 Last visit: 8/17/2024 Posts: 37 Rating: (1) |
Hello, How do we get notification when the Siemens Industrial OS is ready? Thanks David |
2/9/2021 3:01 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, please have a look at this document to setup the example image on an SD card. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on