Industry Online Support
Technical Forum
3/15/2010 10:08 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already püublished in the following thread. How to Interchange the Drive and Motor of one double motor module to another double motor module in Existing Project with Keeping the Relevant parameter of that Drive and Axis in Simotion D435 with Sinamics s120. Best regards O_Moderator |
Follow us on