2/27/2019 6:19 AM | |
Posts: 2826 Rating:
|
Hello Tomy. Thanks to Jay you have one piece of the puzzle. The list of S7-300 that can be programmed with TIA Portal is very limited. Only new firmware versions are covered. HSP (hardware service packs) is the only medium to add devices to Step7 in TIA Portal. What makes things worse is that some PLCs are even removed from the list of possible TIA Portal candidates. For clarity on specific combinations, use the comparability tool: https://support.industry.siemens.com/cs/document/64847781/ BR |
This contribution was helpful to
1 thankful Users |
2/27/2019 5:13 PM | |
Posts: 2826 Rating:
|
Hello. I am not sure what you mean by "both". The operating system of the PC is not really in question - is it? I have gone through the same type exercise defining Step7 TIA and Classic versions. The system also produced another list which I add now. It states more PLCs and software versions. BR AttachmentStandard-CPUs-(S7-300)_compatibility-list_en_2018-12-12.zip (93 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on