12/6/2016 9:53 AM | |
Posts: 1 Rating: (0) |
hi , please advise how to load the S7-300 program into MMR card connecting thru Simatic PG ty ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/6/2016 4:18:04 PMNew subject after splitting |
|
12/6/2016 11:58 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
Oh, I read the FAQ which is from 06/05/2007 and does not include the newer models and therefore is outdated. As well as that not all my mentioned questions are answered. Sorry. |
~(‾▿‾)~ |
|
12/6/2016 12:20 PM | |
Joined: 5/12/2006 Last visit: 1/15/2025 Posts: 22492 Rating: (3043) |
Hello, which newer models you mean? If you mean S7-1200 / S7-1500 you know that this PLC no longer use a MMC? Regards Christoph |
12/6/2016 12:55 PM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
So you say that there were no new cpus since 2007 when the faq was release. Interesting. I guess with no progress the other questions are not relavant, too |
~(‾▿‾)~ |
|
12/6/2016 1:02 PM | |
Joined: 5/12/2006 Last visit: 1/15/2025 Posts: 22492 Rating: (3043) |
Hi, no o don't say this. but the principle how to handling the MMC/project is exactly the same for all S7-300/S7-400 independed which year the PLC was released. The procedure was changed with the new generation S7-1200/S7-1500 because here the Memory Card Architecture and File System is changed and the cards can be used without any special HW Reader in Windows. For S7-300/S7-400 and the (Micro)MemoryCards the handling everytime the same and not chanced! This was what i say. And that was the thing was asked for!
Christoph |
12/6/2016 1:07 PM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
Not according to the last question asked here and the open questions within the old faq. |
~(‾▿‾)~ |
|
12/7/2016 8:36 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
This might help: |
~(‾▿‾)~ |
|
Follow us on