3/23/2019 3:40 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Im not sure whether this could help you slightly or not. In the Alarm logging, you can actually edit something to make your outcome. @102%s@ is the login username. You could play around with it and let us know. Attachment20190323_UserLoginData.zip (80 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/25/2019 9:27 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello mrich, maybe this FAQ can help also Showing logged-in user on a MultiClient. With regards |
3/25/2019 2:44 PM | |
Joined: 5/20/2009 Last visit: 3/14/2022 Posts: 32 Rating: (5) |
Thanx for your respons Heisenberg2, But your suggestion leads to a solution for displaying the logged-in user on a multi-client. That's not my challenge... I wan to see the logged-in user for connected clients on another machine (the OS-server)... Thanx anyway fot showing interest! Regards, Marcel |
3/27/2019 9:08 PM | |
Joined: 2/1/2010 Last visit: 9/25/2024 Posts: 150 Rating: (71) |
I am recently facing a similar request from a customer about how to display what user is logged in at a particular remote client station in real time and thinking about how to do this as well. Taking JOTST's answer and combining with some other system settings, I have an untested concept. If you are using either Maintenance Station or Lifebeat Monitoring in your OS project, you will already have an OPC group/channel in your OS server tags list for each OS client. If you aren't using either one, you should just be able to make the OPC group/channel manually on the server for each client. So the tags will be on the OS server so IP21 is happy with going just one place to grab data. My idea is that you can just manually add a tag for each client to the OPC tag connection list on your OS project under each clients OPC group/channel and give it the remote WinCC OPC address of the client @CurrentUser tag. Following Maintenance Station tag name generation, (of course you can call it whatever you want) the tag could be something like @Client1_@CurrentUser, <text tag type>, with the OPC address needs filled in something like "@CurrentUser","",8. If you try it before me, let me know if it works. |
If my post helped you, please rate. Thanks. |
|
Follow us on