4/6/2023 6:10 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33882 Rating: (4215)
|
Import of a technical question of the userMaxant via PM. Hello, I research solution for reset LOGO 6ED 1052 XXX 0BA1, (equipment buy on the net from un individual), Problem: the logo module stay on RUN mode & password unknown, 1. connect IP address OK (PC ping et LSC V8.3 test connect OK) 2. test reset with LSC tools functions: stop logo, reset manufacture, reset program & password: all conditions necessary password for next step, (I am not the password) 3. I would transfert a new program with SD card, but LSC demand IP address valid for tranfert (add address valid) but LSC transfert directly/research logo module not SD card... (logo on OFF or ON, with or not cable connected: failure are similar) Have you other solution for this problem? Thanks you |
This contribution was helpful to1 thankful Users |
4/6/2023 6:14 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33882 Rating: (4215)
|
Use the Reset Tool. |
Follow us on