10/7/2006 9:24 PM | |
Posts: 5822 Rating:
|
Hello Ahmed, Look also at: Loadable Driver CP 441-2 MODBUS Protocol RTU Format S7 is Slave |
10/8/2006 10:30 AM | |
Joined: 1/7/2006 Last visit: 3/9/2025 Posts: 2705 Rating:
|
Hi Ahmed, When you have the CP 341 Modbus Slave loadable driver then it is very easy to program a Modbus RTU slave. You have to import the FB80 from the installed Modbus Library. See also Modbus Networkfor more information about all kind of software that have direct contact with the Modbus Slave (PtP software and Modbus RTU Slave Software).[;)] When you still have questions, please ask them then on this thread... [:)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
9/11/2012 1:27 PM | |
Posts: 19 Rating:
|
please some help me with a ample project....
|
9/11/2012 1:36 PM | |
Joined: 12/1/2009 Last visit: 2/9/2025 Posts: 672 Rating:
|
Dear sorooshi , sample projects are available with the installation of the loadable driver already. Regards. |
Give us your feedback and show us your respect! |
|
Follow us on