8/19/2020 8:49 PM | |
Posts: 13 Rating: (0) |
hello; I am facing problem in locating Festo pneumatic valve on Step 7. in hardware window when click on Festo module it shows address e.g. 104 to 107 ( digital output as per drawing ) but when I search in program or cross reference sheet. it is not visible. communication is via profibus, Siemens plc s7 300 and step 7 festo valve : CPX- FB 13 pls note appropriate GSD file is already installed. Can any one help to define or any manual as help to understand how to operate (read/write) Festo valve on profibus. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/20/2020 10:02:16New subject after splitting |
|
8/19/2020 11:02 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating: (2678) |
Hello Umair; Please show us a screenshot of the hardware configuration of your Festo CPX-FB13, including all pneumatic valves, so we can see how the addressing is distributed on the modules. And please compare you configuration with the samples in the Festo manual below, it might give you an idea of the relationship between the CPX module and the Profibus addressing (starting on page page 2-30): https://www.festo.com/net/SupportPortal/Files/407534/CPX-FB13_2008-11c_526428g1.pdf Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
8/20/2020 9:02 AM | |
Posts: 13 Rating: (0) |
dear daniel screen shot attached, output 104 to 107 needs to be find and modify in program. regards Umair |
8/20/2020 1:31 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (876) |
Hello, In cross reference check if you could find PQB104, PQB105, PQB106 PQB107 or PQW104, PQW106 or PQD104. |
8/20/2020 4:10 PM | |
Posts: 13 Rating: (0) |
hello daniel thankyou for your support but throught out reference data sheet these I/Os are not visiable. i have attached screen shot. regards Umair |
8/21/2020 4:10 PM | |
Posts: 13 Rating: (0) |
hello daniel; Thanks for reply; i have workout again and now attached file gives you complete picture (i hope). In short my festo valve are attached on this station and particulary i want to excess digital output from 106.3 to 106.6 (squeezer 1 to 4). And yes SFC 14 and 15 are visible. regards Umair Attachment106 squeezerzz.pdf (199 Downloads) |
Follow us on