7/24/2018 9:01 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating:
|
I need to visualize the position of some gear levers on a KPT700 Basic panel. The visualization has already been made in WinCC 7.4 SCADA. Please also see the attached screenshots The bit that contains the information about the gear position is bit 1 in a status word for each possible position of the individual levers. So: The lever 1 will be show in position 1 if bit 1 in the status word for lever 1 in position 1 is high. The lever 1 will be show in position 2 if bit 1 in the status word for lever 1 in position 2 is high. The lever 1 will be show in position 3 if bit 1 in the status word for lever 1 in position 3 is high. The lever 2 will be show in position 1 if bit 1 in the status word for lever 2 in position 1 is high. ETC. I can pick the status word in the HMI tags list - but how do I pick it so that when bit 1 is 1 the color is black and when bit 1 is 0 the color is (backgruond) grey? AttachmentGC.zip (506 Downloads) |
7/24/2018 2:17 PM | |
Joined: 9/21/2012 Last visit: 7/11/2024 Posts: 4006 Rating:
|
My screen shots are from a "VAT table". |
Follow us on