12/9/2011 9:58 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, See attached Lad diagram, it's written in Microwin, but you can use it in any PLC. Regards, Marcjan Attachmenttoggle.pdf (6929 Downloads) |
Problem solved? |
|
This contribution was helpful to11 thankful Users |
12/9/2011 1:24 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (150) |
Thank you for this nice trick, Marcjan |
12/9/2011 1:40 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
AIO (All in One) how to use only one push button to on/off the output (the fastest is a winner) |
This contribution was helpful to1 thankful Users |
12/9/2011 1:42 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, You're welcome. Version in TIA attached, note the extra flag you need for the edge evaluation. Regards, Marcjan @ Umencho, yes that's the shorter one But believe it or not there are still plc's without X-or instruction Attachmenttoggle-tia.pdf (3232 Downloads) |
Last edited by: Marcjan at: 12/9/2011 1:48 PMProblem solved? |
|
12/9/2011 1:59 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (150) |
Thank you, yet better. |
12/9/2011 5:21 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349) |
How does one code this solution in TIA Portal without SCL? |
science guy |
|
12/10/2011 2:31 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
<OFFTOPIC> Just on target! huggy_d1 give us your tip concerning that issue. BTW, do you think that is need to think about that, because around Christmas we expect released of SP2 of TIA v11 coming with SCL. Best regards, Hristo Mihalev |
10/20/2017 2:03 PM |
|
Posts: 1 Rating: (0) |
My solution is very easy :-) try it |
Follow us on