Industry Online Support
Technical Forum
6/2/2010 2:52 PM | |
Joined: 9/27/2006 Last visit: 6/7/2024 Posts: 12260 Rating: (2670)
|
Hello Kkris; Here you can have a look at theIE/As-i link manual: http://support.automation.siemens.com/WW/view/en/22712154 Chapter 7 describes the data exchanges with an As-I slave. This FAQ shows how to integrate an As-I bus to a Profinet master with the IE/As-I link gateway. Besides the documentation, you will also be able to download a sample Step 7 project that will help you develop your application. http://support.automation.siemens.com/WW/view/en/24057268 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/2/2010 2:55 PM |
|
6/5/2010 5:24 PM | |
Joined: 9/27/2006 Last visit: 6/7/2024 Posts: 12260 Rating: (2670) |
Hello Kkris; From the title of your thread, and the text of your earlier post, it was difficult to inderstand that the issue was not with the data transfer, but the diagnostics of the bus. It is easier to helps you if you define your question better at the start. Siemens proposes an Application Note on the IE/AS-i link in the following webpage, including diagnostic functions. You might find it useful to develop your own application: http://support.automation.siemens.com/WW/view/en/24057268 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
6/11/2010 7:41 AM | |
Posts: 4 Rating: (0) |
Hi dchartier, Thanks for your help...
|
Follow us on