7/24/2010 1:22 AM | |
Posts: 4 Rating: (0) |
How I can read the temperature value measured by the AM 2 Pt100 module? give me an example? thanks
|
7/25/2010 5:09 AM | |
Posts: 153 Rating: (15) |
Hi_alainsc 1. To choose an analogue input on which it is connected рт100. 2. To connect to an analogue input the necessary analogue block.3. In parametres of the analogue block to expose parametre рт100. 4. To create block with text message. 5. In parametres of the text message to find the block and the parametre specifying real temperature AttachmentPt100_str.zip (535 Downloads) |
7/25/2010 11:46 AM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi, look my answers at AM2 PT100 °C precision to geta solution with the best possible resolution of the temperature.... Best regards Betel _________________________________________________ Perhaps helpful links: |
==> Meine TAG-Listen: "deut." |
|
Follow us on