4/25/2018 11:09 AM | |
Posts: 4 Rating: (0) |
Dear Sir/Ma, I just bought Siemens Simatic Panel P/N: 6AV36I7-1JC20-0AX1 for the purpose of replacing the old one in the power plant of my customer. The client wants me to replace the old unit with the new one but he said I would need to install a something on the new one in order for it to work. Can the new one work without installing anything on it? I need steps to take to enable me replace the old unit with the new one and at the same time work perfectly without any issues This is the first time I will be buying the panel for the client and part of my work is to replace the old unit with the new one but I dont know how to achieve the task. I have attached the data sheet of the simatic panel for clarification purpose. Can anybody help me and put me through ------------------------------------------------------------------------------------------ AttachmentMicroprocessor Simatic Panel Dta Sheet.pdf (297 Downloads) |
Last edited by: Jen_Moderator at: 4/25/2018 1:24:09 PMNew subject after splitting |
|
4/26/2018 8:41 AM | |
Joined: 4/24/2006 Last visit: 6/6/2024 Posts: 8674 Rating: (1158)
|
Hello, Do you have to replace the same panel? Then you can perhaps use Prosave to backup project of 'old' panel and restore it in the 'new' panel. How to Backup and restore a program on a text or graphic-based panel? Best regards, Wizard |
Last edited by: Wizard at: 4/26/2018 8:42:31 AM |
|
Follow us on