4/9/2022 7:15 AM | |
Joined: 12/18/2014 Last visit: 6/18/2024 Posts: 33206 Rating: (4108) |
You can query the panel's life bit. SIMATIC WinCC WinCC Advanced V14 SP1 - CommunicationIf the life bit stays high or low for more than 2 seconds, the connection to the panel is broken. |
11/21/2022 11:46 AM | |
Joined: 2/17/2018 Last visit: 1/1/2024 Posts: 4 Rating: (0) |
Is it Possible to read broken hmi connection in plc |
Follow us on